FB#.MONITOR#.DATA

Description

Once a signal source is set with the command FB#.MONITOR#.SOURCE, this command can be used to read the value of the signal.

The read value is the same as in the commands FB#.HALLSTATE, FB#.SIGNALAMPLITUDE, FB#.SIGNALSIN and FB#.SIGNALCOS with the difference that it can be recorded.

These commands are only used for FB1 (on the X1 connector) and FB2 (on the X2 connector) when a Smart Feedback Adapter (SFA) is used. The number of monitors is system dependent and two monitors are created by default.

Example

Usage

In the example code below, the source to Cosine is set and checks the value of the signal, both with this command and with FB2.SIGNALCOS.

Since this command can be used to display both Hall State (which does not have any units) and Voltages, this command does not display the units. However, the units are the same as those displayed by the command for the corresponding source.

-->FB2.MONITOR2.SOURCE 4

-->FB2.MONITOR2.DATA

0.314

-->FB2.SIGNALCOS

0.314 [V]

Versions

Action Version Notes
Implemented 02-04-05-002

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

0.000

Data Type

Float
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
FB1.MONITOR1.DATA

3500h

15h

Signed32

-

1000:1

Read only

Yes

FB1.MONITOR2.DATA

3500h

16h

Signed32

-

1000:1

Read only

Yes

FB2.MONITOR1.DATA

3501h

15h

Signed32

-

1000:1

Read only

Yes

FB2.MONITOR2.DATA

3501h

16h

Signed32

-

1000:1

Read only

Yes

Related Topics

FB#.HALLSTATE

FB#.SIGNALAMPLITUDE

FB#.SIGNALSIN

FB#.SIGNALCOS

FB#.MONITOR#.SOURCE